Press Suppliers
Press Suppliers
DC-Motors for compact drives for Hexapod micropositioning systems

Compact industrial robots

The miniaturization of mechanical, electrical and electronic components is one of the key trends dominating research and development activities within the area of miniature drive technology. To be able to measure structures in the sub-micrometer range reliable, specialist know-how is essential; simply adopting a downsized standard solution from the „big world“ is not an option. Small yet high-powered motors from FAULHABER are perfectly capable of exploiting new opportunities in automation technology.

Ultra-fine motion control in the production of high-purity crystals and in focusing, scanning, adjustment, inspection and measurement tasks in the sub-μm range demands highly accurate, reproducible movements. The conventional approach to this is to run the object being measured past a measuring probe or actuator on a linear positioner. Piezo drives are known for their capacity to deliver ultra-fine step widths, but unfortunately their dynamism is insufficient to transport the payload into the work area. The traditional solution means minutes of approach work to reach the measuring position. But long setup times cost money. A patented solution for this dilemma uses a geared FAULHABER DC motor for fast transport over long distances. The fine adjustment is being handled by a high precision piezo motor.

Another example of a compact industrial robotic positioning system where FAULHABER is driving miniaturization is the so called Hexapod. These systems are based on six high-resolution actuators that control a single platform. Instead of hydraulic drives, hexapods are powered by high-precision drive spindles and precisely controllable electrical motors. In order to achieve the high positioning accuracy required, the drive systems must also work as backlash-free as possible over the complete operating period.

When it comes to such and other challenging applications, FAULHABER’s standard range of DC precision motors is always primed for action. The self-supporting, ironless rotor coil with a skew-wound design and precious metal commutation provides very favorable preconditions for such areas of application. For example ensuring immediate and high-torque start-up of the DC motors after a voltage is applied. The small, light-weight DC drives furthermore work reliably in adverse environmental conditions.

DC-Motors for compact drives for Hexapod micropositioning systems
Ultra-fine motion control
Highly accurate, reproducible movements
Zero backlash
High reliability and long service life
DC-Motors in robotics Hexapod micropositioning with maximum manoeuvrability and precision
Application
DC Motors
Industry & Automation
Robotics
Compact drives for hexapod micropositioning systems

The miniaturization of mechanical, electrical and electronic components is one of the key trends dominating research and development activities within the area of drive technology. Small yet high-powered motors are capable of exploiting new opportunities in automation technology. One area that has…

Related articles

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.