Nieuws & evenementen

FAULHABER motors in NASA research satellites

In NASA's "Magnetospheric Multiscale (MMS)" research project, motors from FAULHABER will help in examining the earth's magnetic field. The MMS mission should for the first time provide a...

meer

Swiss Engineering Ticino Award

The SWISSENGINEERING TICINO Prize was awarded for the first time in 2007. It is awarded to graduates of the SUPSI (Scuola Universitaria Professionale della Svizzera Italiana) – a technical college –...

meer

Changes in the FAULHABER Distribution Channels

Dear Customers and Partners,

Effective as of July 1st 2015 the exclusive sales contract with Minimotor Benelux BVBA in Luxembourg, Belgium, and the Netherlands, will end. Thereafter we intend to...

meer

SWR Landesschau mobil zu Besuch bei FAULHABER

Zu Gast bei FAULHABER war Moderatorin Sonja Faber-Schrecklein und ihr Team, um ein Interview mit Dr. Fritz Faulhaber zu führen. Im Rahmen der Landesschau mobil berichtete der SWR eine Woche lang über...

meer

Catalogue 2015

Comprising 472 pages, the latest FAULHABER catalogue 2015 includes details of our extensive range of miniature drives and micromotors. Featuring well-presented performance tables and comprehensive...

meer

Integrated encoder IEH3‐4096

The new IEH3‐4096 series from FAULHABER is the most compact 3‐channel encoder of its class. The new model delivers two square‐wave signals as well as an additional index channel. It offers a higher...

meer

Brushless DC-Servomotor Series 3274...BP4

In the fight for high performance with minimum weight, FAULHABER with the development of its series 3274 BP4 has put a new champion in the ring. The brushless DC servomotor, measuring 32 mm in...

meer

MCST 3601 drive electronics for stepper motors

Searching the multitude of available programmable motion controllers for a controller that is ideally suited to miniaturised stepper motors with phase currents of sometimes less than 100 mA was once a...

meer

New FAULHABER motion

In this issue of our FAULHABER motion magazine we illustrate in no uncertain terms the variety of applications our products find a home in. Applications of FAULHABER products from deep space to...

meer

6.5 billion kilometers to the workplace

At the end of May 2014, the Rosetta space probe will swing into an orbit around the comet 67P/Churyumov‐Gerasimenko in order to, after more closely approaching it in August, map its surface and thus...

meer

FAULHABER verleiht Lieferanten-Award an Stanztronic GmbH & Co. KG

FAULHABER verleiht am 17. September in Schönaich erstmals einen Award für die beste Leistung von Lieferanten. Preisträger ist die Stanztronic GmbH + Co KG aus Remchingen, die Werkzeuge für...

meer

Auszubildende 2014

Wir freuen uns, unsere neuen Auszubildenden 2014 begrüßen zu dürfen. Nach einer Woche IHK-Seminar zum Ausbildungsbeginn und einem erfolgreichen Einführungstag ging es am 9. September 2015 richtig los!...

meer

FAULHABER honoured as "Top Innovator"

For more than 20 years, the "Top 100" emblem has stood for the power of innovation, team spirit and the thirst for knowledge. Once again this year, on June 27 Germany's most successful innovation labs...

meer

Normaler Artikel

Auch gibt es niemanden, der den Schmerz an sich liebt, sucht oder wünscht, nur, weil er Schmerz ist, es sei denn, es kommt zu zufälligen Umständen, in denen Mühen und Schmerz ihm große Freude bereiten...

meer

Stepper motors series FDM0620 - So small, so powerful!

With the new FDM0620 series, FAULHABER presents a stepper motor with minimal size: contained in a housing measuring just 9.7 mm in length and 6 mm in diameter are all components (including the...

meer