• Feel the Power

    FAULHABER Motion Control

    more

  • Engineers, get ready to play

    FAULHABER Motion Control

    more

  • It‘s not a trick. It‘s engineering.

    FAULHABER Motion Control Systems

    more

A new generation

Drive technology plays an important role within the context of networked industry, after all, automation is not possible without a “driving force”. The new approach has far reaching consequences particularly for control technology: decentralised intelligence, capacity for real-time communication with higher level process control technology, maximum compatibility regarding the drive technology used as well as maximum flexibility and scalability with the application areas are the primary requirements of today. FAULHABER has taken appropriate action and developed a new generation of motion controllers which leaves nothing to be desired in this respect.

Decentralised intelligence promotes maximum performance

Not limited to, but perfectly optimised for the ­FAULHABER drive program, you extract the maximum from any FAULHABER drive with the MC 5004, MC 5005 and MC 5010 version positioning controllers – whether DC-Micromotors, Brushless or Linear DC-Servomotors.

more

Well prepared for industrial networks

In addition to the variants enclosed in a housing, the Motion Controller is also available in a version as open plug-in card. In combination with an optionally available motherboard, you can easily control multiple axes in synch via the normal cyclic modes – CSP, CSV and CST – together with, e.g., a higher-level PLC.

more

Direct use in automation environment

It is hard to believe how much intelligent and high-performance drive technology we have conjured up in the compact FAULHABER Motion Control Systems. Their robust construction in accordance with IP 54 meets even demanding industrial requirements.

more