More Power in the Hand

The new 2668 … CR DC motor from FAULHABER offers considerably more power than comparable drives, and is the most powerful copper-graphite commutated DC-micromotor in its size class on the market. Thanks to a bigger NdFeB magnet and a high copper content in the winding, it supplies a rated torque of 70 mNm. As a result, it weighs just 189 g with a diameter of 26 mm. Furthermore, it reaches full power extremely quickly with its high pulse torque. The 2668 … CR is thus especially well suited for professional high-performance tools such as pruning shears or motorised screwdrivers.

The copper-graphite brushes of the motor are characterised by their outstanding stability and low wear. The housing is made of coated steel. The motor can be combined with high-resolution optical or magnetic encoders. As well as handheld devices, it is also suitable for many other applications such as in aerospace, robotics, medical technology, in special machinery construction, metering systems and automation solutions.

FAULHABER specializes in the development, production and deployment of high-precision small and miniaturized drive systems, servo components and drive electronics with output power of up to 200 watts. The product range includes brushless motors, DC micromotors, encoders and motion controllers. In addition, FAULHABER also offers customer-specific complete solutions for, among others, medical technology, automatic placement machine, precision optics, telecommunication, aerospace and robotics. FAULHABER has more than 1,600 employees worldwide.