Press Suppliers
Press Suppliers
DC-Motors for humanoid service robot that works autonomously

The more human-like a robot should be, the more sophisticated the mechatronic engineering input necessary. ­Particularly in sectors requiring "human social behaviors", e.g. for service functions or providing information in places such as museums, airports or hospitals, sophisticated technology for robot construction is a must. For many years, the Barcelona-based company Pal Robotics S.L. has been working on the construction of humanoid robots for special applications. Non-verbal communication, i.e. body language, also plays an important role in increasing the acceptance of humanoid robots. In order to accommodate as many functions as possible in the predefined robot body, the robotics experts have been working with Schönaich-based microdrive ­specialist FAULHABER. The outcome has been a robot model that most definitely exhibits human traits and is capable of ­emphasizing certain statements by means of "body language".

DC-Motors for humanoid service robot that works autonomously
Sensors and a touch screen allow the robot to move and communicate
DC-Motors for humanoid service robot that works autonomously

Service robots for practical applications.

Humanoid robots intended to perform everyday functions have to satisfy ­certain conditions. The developers wanted to integrate capabilities such as information output, minor transport tasks and service functions into the new REEM robots. This resulted in a robot height of 1.65 m, so that it can communicate with humans at eye level. It was also important that the robot should not be excessively heavy, although there was a need for a low ­centre of gravity and space to house the necessary batteries. The current robot model weighs around 90 kg, sufficient for one set of batteries allowing eight hours of autonomous operation. In addition to its unladen weight, this service robot can also carry up to 30 kg effective load on its lower loading platform. Each arm can move up to 3 kg independently. In this case, wheels located in the base of the robot ensure effective locomotion. On the one hand, this ensures minimal power consumption and quiet running, while on the other the design provides sufficient mobility for the planned application of up to 4 km/h.
As well as a touch screen for the various programmable applications, the REEM is also equipped with microphone, stereo camera, laser and ultrasound sensors, accelerometers and gyroscopes. These devices enable the robot to identify its current position in the room, move around autonomously in its area of work and avoid sudden obstacles or people walking across its path.
Two DC microdrives in the robot's neck and waist provide the necessary expressiveness. Thanks to their compact dimensions, the drives can be readily used even in these two "constricted" areas. The small actuators can move head and torso independently of one another and allow them to assume different postures. This enables the robot to imitate human traits using body language suited to the ­respective situation.

DC-Motors for humanoid service robot that works autonomously
DC-Motors for humanoid service robot that works autonomously

Microdrives offer flexibility.

Microdrives do not just replicate larger motors. Because of the physics involved they often offer better dynamics, higher output or greater efficiency than you would expect as a result of a mere reduction in size. In practice, this means that very high short-term overload capabilities are possible without affecting service life. This proves particularly advantageous when it comes to executing the less frequent but temporary actions necessary to mimic specific gestures. As well as these features typical of all micromotors, the various models come with further benefits depending on the application in hand. Stepper motors offer accurate positioning without additional encoders thanks to a defined step width per control pulse. Brushless drives run even at minimal supply voltages and are thus ideal for autonomous, battery-backed systems that are designed not to fail immediately in the event of a voltage drop. Electronically commutated DC motors represent the best option for long service life and maximum dynamics. Intelligent motion controllers can control the drive in four-quadrant operation and reduce the load on the robot controller. By means of different gear motor combinations, all miniature devices can be set to an application-specific speed or the required output torque. The fact that micromotors have for a long time already been in use in "robotized" aids such as motor-powered hand and leg prostheses shows that they meet the most stringent requirements not just for human robotics.
The range of applications for modern microdrives is very varied, with a wide range of designs available depending on application. In itself, however, this does not yet guarantee universal use under all circumstances. This is where the ­system concept comes into play. It is the extensive range of accessories, from ­control ­modules such as motion controllers, encoders, bus connections, various gear heads and ultimately the adapted, ­flexible control electronics that make microdrives the ideal mechanical ­"muscle" in robot manufacture.

Products

DC-Motors
No cogging
Smooth position and speed control
High efficiency
Low Noise
High Torque
Low Weight
Very low rotor inertia
Dynamic start-stop operation
Details

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.