Originally invented by Dr. Fritz Faulhaber Sr. and patented in 1958, the System FAULHABER coreless (or ironless) progressive, self-supporting, skew wound rotor winding is at the heart of every System FAULHABER DC Motor. This revolutionary technology changed the industry and created new possibilities for customer application of DC Motors where the highest power, best dynamic performance, in the smallest possible size and weight are required.
The main benefits of this technology include no cogging torque resulting in smooth positioning and speed control, higher overall efficiency than other DC Motor types, extremely high torque and power in relation to motor size and weight, and a linear relationship between load to speed, current to torque, and voltage to speed. The very low rotor inertia results in superior dynamic characteristics for starting and stopping and the motors exhibit extremely low torque ripple and EMI.
Diabetes is among the most common diseases in today's societies. If the disease is not treated in time or if treated incorrectly, important organs, such as heart, eyes and kidneys, could suffer serious damage. Chronically ill patients can optimally control their treatment with an...
The corona pandemic has clearly demonstrated to the whole world just what a highly contagious virus can do. Tourists and travellers have unintentionally contributed to the spread of the disease. Detecting infected persons on arrival at airports is key in preventing a potential chain...
Automate brings the greatest minds and solutions in automation together under one roof. Here, you’ll have access to over 20,000 decision makers from around the world—spanning 40+ industries and performing every type of application.
Here you will find external YouTube contents for the article. Click to watch.
I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.