Press Suppliers
Press Suppliers
PiezoMotors power MRI Robot

Guided by real-time feedback, the robot can position a high-energy, interstitial focused ultrasound probe exactly at the tumor, delivering optimal surgical results and an ideal outcome for the patient. Of course, building a robot that can operate within the high magnetic fields generated by an MRI unit was not easy, but with sophisticated controls engineering and piezoelectric positioners from FAULHABER, the WPI team has built a system that promises to revolutionize the treatment possibilities of MRI.

The process of designing surgical devices is rife with challenges. Systems need to be accurate and repeatable, with ultrahigh resolution. They have to be electrically quiet. Above all, they must be reliable. In the case of the MRI robot, Fischer's team faced another enormous challenge: delivering all of these characteristics in a system that can also function in multi-tesla magnetic fields.

The powerful magnetic field generated by an MRI machine makes hazards of even small ferromagnetic objects like screws, let alone, motion devices like permanent magnet motors, gearboxes, and actuators. It was obvious from the outset that the MRI robot had to be based on non-traditional actuation. The answer proved to be a piezoelectric device.

PiezoMotors power MRI Robot
PiezoMotors power MRI Robot

Motion In A Magnetic Environment

Piezoelectric actuators are based on a piezoelectric ceramic that expands under an applied voltage. The problem is that the displacement introduced by the piezo effect is only a fraction of a percent of component size, while the MRI robot required up to about 100mm of linear travel or a continuous 360-degree rotation. The WPI team found the solution in the Piezo LEGS motors from FAULHABER.

The units consist of a set of bimorphic drive legs that are constructed so that under an applied voltage, they flex slightly and extend.

In practice, they are driven in alternating pairs so that they "walk" a drive rod forward in nanometer steps at speeds as high as 15 mm/sec (or spin a disc in the case of rotary motion). Because one set of legs is the always in contact with the actuator at any time, they are inherently safe actuators (providing braking when unpowered) with the motors provide a stall force (holding force) of up to 10 N.

PiezoMotors power MRI Robot
PiezoMotors power MRI Robot
A voltage applied to the biomorphic legs causes them to bend and extend or retract, allowing them to move a drive rod forward.
PiezoMotors power MRI Robot
PiezoMotors power MRI Robot

The WPI robot consists of one module with X, Y, Z translation and two rotational modules that correspond to the arc angles of a head frame. Future designs will include additional of degrees of freedom to permit the insertion and rotation of cannula and stylet.

To generate linear motion, the WPI team uses a combination of linear Piezo LEGS motors in a direct drive for needle insertion and rotary Piezo LEGS motors to drive aluminum lead screws. For rotary motion, they use 3D-printed custom pulleys and rubber- or fiberglass-reinforced timing belts.

Although the masses involved are small, the materials generate greater friction than conventional designs, which means that they require higher torque to produce motion, and the piezomotors deliver. "In a lot of applications, you can get away with a piezo motor and a direct drive or a pulley reduction of several-to-one," Fischer says. "You don't need 100:1 gear ratio reductions like you might need with a small DC motor."

Piezo LEGS turned out to be the right solution for the WPI project. "There are piezoelectric actuators that will give you at best maybe 1mm of motion," says Fischer. "Beyond that, you're really down to only a few companies. Of those, they sell rotary motors or they sell modules that you push up against the drive rod, but you need to actually design a whole custom device around it. In terms of compact and self-contained motors, I haven't seen any competition, really, for the FAULHABER devices."

Control Challenges

The piezoelectric actuator requires only very small conductive electrodes that are both nonmagnetic and non-ferrous; this makes it safe for use in the MRI environment. In this application, however, safe was not enough. Any electrical noise generated by power supply or drive electronics has the potential to distort the image, which would defeat the purpose. "A lot of times you'll get static-like artifacts," says Fischer. "Electronic noise coupled with non MRI-compatible materials can effectively warp the image and then things won't show up where you expect them to which is a major, major problem if you're trying to guide an intervention based on the imagery."

PiezoMotors power MRI Robot

Clearly, the application required specialized electronics. At the same time, the nature of the piezoelectric motor meant that it required a sophisticated drive waveform. In response, Fischer's team developed a custom control package for operating piezoelectric motors in the MRI scanner. They programmed a field-programmable gate array (better known as an FPGA) to adjust the relative frequency and phase of the drive signal waveforms. High-speed digital-to-analog converters deliver precise temporal control of the waveform, and high-bandwidth, high-voltage linear amplifiers allow the controller to synthesize the exact drive signal needed to produce the motion. External filters remove noise, and encoder feedback enables closed-loop position or velocity control from a microcontroller running a real-time control loop on a single board. A modular backplane combines up to eight of these boards into a single shielded enclosure that resides inside the MRI scanner room with the robot. A custom cabling harness connects the controller with the robot for up to eight axes of control.

It was not a controls challenge for the faint of heart, but the project was simplified by the availability of a standalone piezo motor. "Having a reliable, ready to go, closed actuator, linear or rotary, has been a big advantage," says Fischer. "It has really let the students focus on the mechanical mechanism design and the controller design." The project goes beyond just the surgical robot, though. Fischer's goal is to develop a toolbox for developing MRI-compatible robots that would incorporate sensors, actuators, controllers, and amplifiers enhanced with communication protocols. "In this industry, you can buy a PLC or motor or an encoder, plug them all together, and you immediately have a working device," he says. "There's nothing really like that for medical devices and there's definitely nothing close to that for MRI."

To demonstrate the approach, the team is working on variations of the MRI robot for several applications including: high-precision thermal ablation of deep brain cancer, deep brain stimulation electrode placement for Parkinson's disease, and targeted MRI-guided prostate cancer biopsy and localized therapy delivery. "We're shooting for very compact, very application specific, and they're all based on these motors," he says. "I have just about every piezo motor on the market in my lab. We have even tried to make our own. For us, the FAULHABER actuators were a very good size with good force ranges, and very good torque ranges. Overall they have been very effective."

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.