Press Suppliers
Press Suppliers
Montion Controllers in compact measuring device from Q-tec GmbH

Material properties testing

The ranger always has her binoculars with her so that she can check wildlife populations or take a close look at the tree tops, for example. The housing, which is subject to heavy wear, is protected by an anodized coating that is only a fraction of a millimeter thick but is nevertheless incredibly hard and robust. Its hardness, and therefore its quality, was tested by the manufacturer using a special device. The precisely measured force applied by a FAULHABER motor plays a crucial role in this process.

The hardness of a material is one of its key properties. A wide range of procedures can be used to test hardness, including the Vickers, Brinell, Rockwell, Knoop and Shore A hardness tests. For example, the latter is used for components made from elastic polymers: A testing probe presses against the material with a defined force. Electronically commutated DC-servomotors precisely control the force applied. With an integrated Motion Controller and a corresponding communication interface, they form the mechanical link between the measuring computer and the probe.

In other testing tasks too, such drives are used to perform precise movements, for example when positioning sample mounts in three dimensions, moving the turret of testing tool magazines or aligning optical components.

The compact drives must fit in the smallest testing devices and allow intermittent start/stop operation with zero vibration. The graphite-commutated motors of the CR and CXR series in combination with IE3 encoders and planetary gearheads are among the drives particularly well suited to such tasks. In addition to high power from an extremely small volume, they offer a very high resolution. In addition, the position of reference marks and limit switches can be taken into account.

Very similar requirements apply when testing other material properties such as the viscosity of flowing media. It is determined in a measuring pot with a rotating paddle. The viscosity changes the resistance and therefore the torque of the drive. Using DC-servomotors from FAULHABER, for example from the brushless series 4490 … BS, the torque can be read with high precision and repeatability. The integrated, linear Hall sensor enables low speeds. The motor runs without a cogging torque and with an absolutely linear ratio of voltage to speed and current to torque. If desired, FAULHABER can provide the drives as a complete package including motor, gearhead, encoder, brake and controller from a single source.

Montion Controllers in compact measuring device from Q-tec GmbH
Highest precision and reliability
Smooth adjustment speeds
Minimal installation space
High level of accuracy
Brushless Motors for ViscoQuick test device
Application
Brushless DC-Motors
Drive Electronics
Metrology & Testing
Motion Controller
Delicate glaze firmly in grip

From smooth and creamy to light and fluffy to thick and sticky – with foods, our mouthfeel provides reliable information about consistency. Spit out or swallow? We make this decision in just a fraction of a second. In industry, one would gladly have decisions that could be made as quickly and…

Related articles

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.